5G NR

Channel Setup UL-SCH

The uplink shared channel (UL-SCH) is a transport channel for PUSCH. Its purpose is to provide user data, channel reports, and RRC setup information.

This topic describes the following UL-SCH properties:

Channel Editor

Add UL-SCH

Delete UL-SCH

Copy UL-SCH

UL-SCH Count

General Settings

Name

Enabled

Power Boosting

Scrambling

Transform Precoding

RNTI

n_ID

n_RAPID

Transmission Settings

Antenna Port(s) Generated

Codebook-Based Transmission

DMRS port(s)

Number of Layers

Number of Antenna ports

Number of DMRS CDM groups without data

Number of Codewords

TPMI Index

Resource Allocation

Allocated Slots

First Symbol

Last Symbol

Bandwidth Part

RA Type

RB Offset

RB Number

RBGSize

RBGBitmap

RB Number Restriction

RB-Set Start

RB-Set Number

Interlace Index

Unused RB

Frequency Hopping Mode

RB Offset Between Frequency Hops

RateMatchPattern(s)

Modulation and Coding

Channel Coding

MCS Table

MCS

xOverhead

Number of Slots for TBoMS

Start Position for LDPC Rate-Matching

Coding Rate

Modulation

User Defined Constellation

Format of the Constellation String

Transport Block Size

BaseGraph

LBRM

Payload Data

Custom Pattern

User File

Modulation and Coding (Transport Block 2)

MCS #2

Coding Rate #2

Modulation #2

Transport Block Size #2

BaseGraph #2

Payload Data #2

Custom Pattern

User File

HARQ Settings

RV index

CBG Transmission

Max CBGs Per TB

CBG Transmission Information

Channel Setup UL-SCH

CRC Error Flag

DMRS Settings

DMRS-Uplink-r16

DMRS-UplinkTransformPrecoding-r16

n_SCID

N_ID_0

N_ID_1

DMRS Power Boosting

DMRS Configuration

DMRS Duration

Enhanced DMRS Type

DMRS-add-pos

PUSCH Mapping

DMRS-typeA-pos

n_ID_RS

Group Hopping

Sequence Hopping

PTRS Settings

PTRS Enabled

PTRS PowerBoosting

PTRS port(s)

Frequency Density (K_PTRS)

Time Density (L_PTRS)

PTRS RE Offset

Number of samples per PT-RS group

Number of PT-RS groups

N_ID

UCI on PUSCH

UL-SCH Enabled

uci-on-pusch-scaling

HARQ-ACK

Enabled

Payload Data

Custom Pattern

User File

Payload Size

BetaOffsetIndex

CSI1 or CSI2

Enabled

Payload Data

Custom Pattern

User File

Payload Size

BetaOffsetIndex

CG-UCI

Enabled

Payload Data

Custom Pattern

User File

Payload Size

BetaOffsetIndex

Channel Editor

Many of the channel types described in this topic provide a convenient channel editor, in table format, for convenient viewing and configuring of multiple channels. The for adding, removing, and copying rows appear directly above the editor. As you make edits, the Channel Allocation graph updates and, if a channel conflict occurs, an error message appears, describing the conflict.

Add UL-SCH

Adds an uplink control channel. This inputted parameter is optional. Supports up to 32 channels.

See also, Adding, Copying, and Deleting BWP or Channels.

GUI Location

Apps > 5G NR > Carrier > UL > Uplink > UL-SCH > + sign to Add

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH:ADD SCH|RTRansmission

SCPI Example

RAD:NR5G:WAV:CCAR0:ULIN:SCH:ADD

Delete UL-SCH

Deletes the selected UL-SCH channel from the setup table.

See also, Adding, Copying, and Deleting BWP or Channels.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Ellipsis icon > Delete

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH:DELete <integer>

SCPI Example

RAD:NR5G:WAV:CCAR0:ULIN:SCH:DEL 1

Copy UL-SCH

Copies the currently selected UL-SCH channel to the last column of the setup table. Supports up to 32 channels.

See also, Adding, Copying, and Deleting BWP or Channels.

GUI Location

Apps > 5G NR > Carrier > UL > Uplink > UL-SCH> Ellipsis icon > Copy

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH:COUNt?

SCPI Example

RAD:NR5G:WAV:CCAR0:ULIN:SCH:COPY 1

UL-SCH Count

Displays the available UL-SCHs.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > UL-SCH Count

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH:COUNt?

SCPI Example

 

Preset

1

State Saved

No

General Settings

Name

Sets the name of the UL-SCH channel.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > General Settings > Name

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:NAMe <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:NAMe?

SCPI Example

 

State Saved

Yes

Enabled

Enables or disables the state of the selected UL-SCH.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > General Settings > Enabled

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>[:STATe]?

SCPI Example

 

Preset

On

State Saved

No

Power Boosting

Sets the additional power boosting for the channel.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > General Settings > Power Boosting

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:POWer <rel_ampl>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:POWer? [MAXimum|MINimum]

SCPI Example

 

Preset

0 dB

Min

-40 dB

Max

40 dB

Resolution

0.01 dB

Scrambling

Enables or disables scrambling for the selected channel.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > General Settings > Scrambling

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:SCRambling[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:PUCCh:SCRambling[:STATe]?

SCPI Example

 

Preset

On

State Saved

Yes

Transform Precoding

Enables or disables Transform Precoding. When enabled, transform precoding is used for uplink waveforms (DFT-s-OFDM waveform type) instead of CP-OFDM.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > General Settings > Transform Precoding

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:TPRecoding[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:TPRecoding[:STATe]?

SCPI Example

 

Preset

Off

State Saved

No

RNTI

Specifies the Radio Network Temporary Identifier (RNTI). RNTIs are used to differentiate or identify a connected UE in the cell, a specific radio channel, a group of UEs in case of paging, a group of UEs for which power control is issued by the eNB, or system information transmitted for all the UEs by 5G gNB.

Refer to 3GPP specifications 38.321.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > General Settings > RNTI

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:RNTI <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:RNTI? [MAXimum|MINimum]

SCPI Example

 

Preset

1

State Saved

Yes

Min

0

Max

65535

Resolution

1

n_ID

Sets the n_ID value for sequence generation. Entering -1 means cell ID.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > General Settings > n_ID

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:NID <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:NID? [MAXimum|MINimum]

SCPI Example

 

Preset

-1

State Saved

Yes

Min

-1

Max

1023

Resolution

1

n_RAPID

Sets the n_RAPID for sequence generation. Entering -1 means not configured.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > General Settings > n_RAPID

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:NRAPid <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:NRAPid?

SCPI Example

 

Preset

-1

State Saved

Yes

Min

-1

Max

63

Transmission Settings

Antenna Port(s) Generated

Specifies the mapping between the physical antennas and the logical antenna ports. Set the number of physical antennas with Total Number of Antennas under the Waveform tab. The logical antenna ports are expressed as P0, P1, P2, P3 and so on.

Enter a comma-separated string or click the arrow to open an editor where you can set the mapping between physical antennas and logical antenna ports. .

For Uplink multi-users MIMO scenarios, multiple UL-SCHs can occupy the same time-frequency resource element (RE) under different physical antenna output. For example, UL-SCH0 uses physical antenna 0 and physical antenna 1 and UL-SCH1 uses physical antenna 2 and physical antenna 3. These two UL-SCHs can occupy the same RE. .

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Transmission Settings > Antenna Ports Generated

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:APORts:GENerated <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:APORts:GENerated?

SCPI Example

 

Notes

Using ‘,’ as delimiter to separate logic antenna port.

Using strings "None","P0","P1","P2","P3" represents none logical port, logical port 0, logical port1 and logical port2 and logical port3.

Such as "P0,P2" means logical port 0 maps to antenna 0 and port2 maps to antenna 1.

Couplings

The number of input ports is the same as Total Number of Antennas under waveform setup node.

Preset

"P0"

State Saved

Yes

Codebook-Based Transmission

Enables or disables a Codebook-Based Transmission.

The range is based on the Number of Layers and Number of Antenna Ports. When Codebook-Based Transmission is Off, the Number of Layers is same as the Number of Antenna Ports. When Codebook-Based Transmission is On, the Number of Layers can be equal to or smaller than the Number of Antenna Ports. See 6.3.1.5 in 38.211 for more information.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Transmission Settings > Codebook-Based Transmission

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CBOok:TRANsmission[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CBOok:TRANsmission[:STATe]?

SCPI Example

 

Preset

Off

State Saved

No

DMRS port(s)

Sets the DMRS port(s) reserved for the transmission of this channel. Multiple DMRS antenna ports can be indicated, using syntax like "0,1,2,3" or "0:3." The Number of Layers is automatically coupled with the number of DMRS ports.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Transmission Settings > DMRS Ports

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:PORTs <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:PORTs?

SCPI Example

 

Notes

There are two ways to configure:

By individual index, use ',' as the delimiter, e.g. 0,1,2.

By a range of index, use ':' to indicate the start index and the last index, e.g. 0:2 means 0,1,2

Couplings

Max number of ports is 4.

DMRS duration is Single Symbol:

    DMRS Configuration is Type 1:

    Max value is 3

    DMRS Configuration is Type 2:

        Max value is 5;

DMRS duration is Double Symbol:

    DMRS Configuration is Type 1:

    Max value is 7

    DMRS Configuration is Type 2:

        Max value is 11

Preset

"0"

State Saved

Yes

Number of Layers

Displays the number of layers for UL-SCH. It is automatically coupled with the DMRS port(s).

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Transmission Settings > Number of Layers

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:LAYers:COUNt?

SCPI Example

 

Preset

1

Resolution

1

Number of Antenna ports

Displays the number of antenna ports used for transmission. It is automatically coupled with the antenna port set.

For UL-SCH, when a codebook-based transmission is enabled, it can be set, but should not be smaller than the Number of Layers.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Transmission Settings > Number of Antenna Ports

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:APORts:COUNt <integer> 

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:APORts:COUNt?

SCPI Example

 

Choices:

1 | 2 | 4

Couplings

When Codebook-Based Transmission is Off, the value is the same as number of layers.

When Codebook-Based Transmission On, set the value smaller than the Number of Layers.

Preset

1

Min

1

Max

4

Number of DMRS CDM groups without data

Sets the number of DMRS CDM groups without data, which is used to determine how many resource elements are reserved for DMRS. When this parameter is changed, the DMRS power boosting is automatically coupled based on table 4.1-1 of 38.214.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Transmission Settings > Number of DMRS CDM Groups Without Data

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:CGWData:COUNt <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:CGWData:COUNt?

SCPI Example

 

Couplings

Transform Precoding On:

Read-only; Value is 2;

Transform Precoding Off:

    DMRS Configuration Type 1:

    Max value is 2; Min value is coupled with DMRS Port(s)

    DMRS Configuration Type 2:

        Max value is 3; Min value is coupled with DMRS Port(s)

Preset

1

State Saved

Yes

Min

1

Max

3

Resolution

1

Number of Codewords

Displays or returns the antenna ports index codeword number.

When the number of DMRS ports is less than or equal to four, only one codeword is supported.

When the number of DMRS ports is greater than four, two codewords are supported..

The Two Codewords support requires license version 2024.0801 or later.

When Number of Codewords is 2, a new category "Modulation and Coding (Transport Block 2))," comprising six new parameters, is added. These new parameters are appended with “#2” to distinguish them from those of Transport Block 1. Likewise, few parameters of Transport Block 1 are appended with “#1.” (.)

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Transmission Settings > Number of Codewords

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH:CWORds:COUNt?

SCPI Example

RAD:NR5G:WAV:CCAR0:ULIN:SCH:CWOR:COUN ?

Preset

1

State Saved

Yes

TPMI Index

Transmitted Precoding Matrix Indicator (TPMI) sets the TPMI Index when Codebook-based Transmission is enabled, the range is based on the number of layers and number of antenna ports

Number of Layers Number of Antenna Ports Valid value for TMPI Index
1 2 0-5
2 2 0-2
1 4 0-27
2 4 0-21
3 4 0-6
4 4 0-4

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Transmission Settings > TRMI Index

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:TPMI:INDex <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:TPMI:INDex? [MAXimum|MINimum]

SCPI Example

 

Couplings

Codebook-Based Transmission On:

Number of Antenna Ports is 1:

    Read-only; Value is -1

Number of Antenna Ports is 2:

    Settable; Min value is 0

    Number of Layers is 1:

        Max value is 5

    Number of Layers is not 1:

        Max value is 2

Number of Antenna Ports is 4:

    Settable; Min value is 0

    maxTpmi = {27, 21, 6, 4 }

  Max value = maxTpmi[Number of Layer - 1]

Other antenna ports number:

       Settable; Value is 0

Codebook-Based Transmission Off:

    Read-only; Value is -1

Preset

-1

State Saved

Yes

Min

-1

Resolution

1

Resource Allocation

Allocated Slots

Sets the allocated slot index for the channel. Allocated Slots are entered as an array of slot indexes allocated for the PUCCH. There are three ways to configure:

These three configuration methods can be used in combination, by using ',' as the delimiter, e.g. 0,1,4:7,8:2:19 means index 0,1,4,5,6,7,8,10,12,14,16,18.

If the slot allocation is different for different frame, use '{ }' and '|' to specify the frame index, for example, {0|0,1,2},{1|3,4,5} means slot 0,1,2 for frame 0, and slot 3,4,5 for frame 1. Ensure the Number of Radio Frames under Waveform Setup node is large enough.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Resource Allocation > Allocated Slot

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:SLOTs  <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:SLOTs?

SCPI Example

 

Couplings

The range of slot index is from 0 to number of slots in the frame of current numerology - 1.

The number of slots in the frame is coupled with the numerology used by this channel, which is defined in the selected BWP. Refer to the Frame Structure table for the details about the relationship between number of slots in the frame and numerology.

Preset

"0:19"

State Saved

Yes

First Symbol

Sets the first symbol index for the transmission.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Resource Allocation > First Symbol

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:SYMBol:FIRSt <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:SYMBol:FIRSt? [MAXimum|MINimum]

SCPI Example

 

Couplings

For Normal CP the maximum value is 13

For Extended CP the maximum value is 11

Preset

0

State Saved

Yes

Min

0

Max

13

Resolution

1

Last Symbol

Set the last symbol index for the transmission.

The range may also be determined by the DMRS location, see more information about DMRS in 38.211.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Resource Allocation > Last Symbol

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:SYMBol:LAST <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:SYMBol:LAST?

SCPI Example

 

Couplings

Normal CP max value is 13

Extended CP max value is 11

The min value is the First Symbol.

Preset

13

State Saved

Yes

Min

1

Max

13

Resolution

1

Bandwidth Part

Select a bandwidth part to be used for transmission. All the BWP names defined under BWP Setup node will be listed here.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Resource Allocation > Bandwidth Part

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:BWP 0|1|2|3|4|5|6|7

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:BWP?

SCPI Example

 

Couplings

Coupled with the Number of BWP. For example, if the number is 1, only BWP1 is allowed, if the number is 2, BWP1 and BWP2 are allowed.

Preset

0

State Saved

Yes

RA Type

Sets the resource allocation (RA) type for the transmission. Type 0 uses a bitmap allocation method. Type 1 uses RB Offset and RB Number for allocation.

Only Type 1 is allowed when Transform Precoding is enabled, otherwise an error occurs.

For Type 2 , errors will occur if any of the following conditions are not met:

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Resource Allocation > RA Type

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:RATYpe TYPE0|TYPE1|TYPE2

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:RATYpe?

SCPI Example

 

Preset

TYPE1

State Saved

Yes

RB Offset

Specifies the RB Offset relative to the selected BWP for RA Type1. This value specifies the RB starting point within the containing resource allocation.

RB Offset is only available when RA Type is set to Type 1.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Resource Allocation > RB Offset

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:RB:OFFSet <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:RB:OFFSet? [MAXimum|MINimum]

SCPI Example

 

Couplings

Range: 0 ~ RB Number – 1 (RB Number is under BWP node)

Preset

0

State Saved

Yes

Min

0

Max

272

Resolution

1

RB Number

Sets the number of resource blocks assigned to the channel. This value specifies the contiguous set of RB starting at RB Offset within the containing resource allocation.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Resource Allocation > RB Number

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:RB:NUMBer <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:RB:NUMBer? [MAXimum|MINimum]

SCPI Example

 

Couplings

If Transform Precoding is On, and RB Number Restriction is On and the RB number is restricted to (2^a * 3^b * 5^c) and less than the BWP number.

Otherwise, the maximum value of the RB Number is the selected BWP – RB Offset

Preset

273

State Saved

Yes

Min

1

Max

273

Resolution

1

RBGSize

Specifies the RBG size when RA Type 0 is selected. The choices are determined by the bandwidth part (BWP) size. See table 5.1.2.2.1-1 in 38.214.

This parameter is available only when RA Type is set to Type 0

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Resource Allocation > RBGSize

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:RBG:SIZE <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:RBG:SIZE?

SCPI Example

 

Couplings

When RA Type 0: Settable.

The choices are determined by the bandwidth part size, see table 5.1.2.2.1-1 in 38.214

Max and min values are defined below.

RB Number of selected BWP

Minimum

Maximum

1 - 36

2

4

37 - 72

4

8

73 - 144

8

16

≥ 145

16

16

RA Type 1: Read Only

Preset

16

State Saved

Yes

RBGBitmap

Enter a string of ones-and-zeros or click the arrow to open the where you can assign allocated RBGs for transmission. Allocated RBGs are determined by the RB Number (N_BWP_size) and the RA configuration. Refer to the 5G NR standard (318.214 - 5.1.2.2) for the BWP RBG allocation matrix.

This parameter is available only when RA Type is set to Type 0.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Resource Allocation > RBGBitmap

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:RBG:BITMap <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:RBG:BITMap?

SCPI Example

 

Couplings

RA Type 0: Settable

Length of the string is coupled with RB Number, RB Offset under BWP node, and the RBG Size

Length = (RB Number + RB Offset % RBG Size + RBG Size -1) / RBG Size

RA Type 1: Read Only

Preset

111111111111111111

State Saved

Yes

RB Number Restriction

Enables or disables the RB number restriction when Transform Precoding is enabled. If On, the UL-SCH RB number is restricted to (2^a * 3^b * 5^c) or less than BWP number, where a, b, and c are non-negative integers.

When RA Type is set to Type 2, the lowest-indexed M_RB_PUSCH PRBs will be used.

This function is only available when Transform Precoding is enabled.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Resource Allocation > RB Number Restriction

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:RB:NUMBer:RESTriction[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:RB:NUMBer:RESTriction[:STATe]?

SCPI Example

 

Preset

On

State Saved

Yes

RB-Set Start

Sets the RB-Set Start index used for ULSCH RA Type 2 transmission.

This parameter is available only when RA Type is set to Type 2.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Resource Allocation > RB-Set Start

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:RBSet:STARt <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:RBSet:STARt?

SCPI Example

 

Preset

0

State Saved

Yes

RB-Set Number

Sets the RB-Set Number used for ULSCH RA Type 2 transmission.

This parameter is available only when RA Type is set to Type 2.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Resource Allocation > RB-Set Number

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:RBSet:NUMBer <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:RBSet:NUMBer?

SCPI Example

 

Preset

1

State Saved

Yes

Interlace Index

This parameter is only available when RA Type is set to 2.

Sets the Interlace index used for ULSCH RA Type 2 transmission, multiple values are allowed, such as 0,1,2,3, or 0:3.

A comma-separated string is used to indicate which interlace(s) are used for transmission, there are up to M interlace indices can be used. (M=10 for u=0; M=5 for u=1)

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Resource Allocation > Interlaced Index

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:INTerlace:INDex <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:INTerlace:INDex?

SCPI Example

 

Preset

0

State Saved

Yes

Unused RB

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Resource Allocation > Unused RB

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UNUSed:RB <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UNUSed:RB?

SCPI Example

 

Couplings

This parameter is visible only when RA Type is Type 2.

Preset

0

State Saved

Yes

Frequency Hopping Mode

Set the Frequency Hopping Mode for UL-SCH.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Resource Allocation > Frequency Hopping Mode

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:FHOPping DISabled|INTRaslot|INTerslot

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:FHOPping?

SCPI Example

 

Preset

DISabled

State Saved

Yes

RB Offset Between Frequency Hops

Sets the RB offset between two frequency hops when Frequency Hopping is enabled.

This parameter is only available when Frequency Hopping Mode is enabled.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Resource Allocation > RB Offset Between Hops

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:FHOPping:RB:OFFSet <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:FHOPping:RB:OFFSet?

SCPI Example

 

Preset

0

State Saved

Yes

RateMatchPattern(s)

Opens the RateMatchPattern(s) editor to set the rate match patterns.

Although RateMatchPattern is a Cell Level or BWP Level setting, the RateMatchPatterns defined under each UL-SCH are only applied to the selected UL-SCH.

Modulation and Coding

Channel Coding

Enables or disables transport layer channel coding.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding > Channel Coding

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CCODing[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CCODing:[:STATe]?

SCPI Example

 

Preset

On

State Saved

Yes

MCS Table

Specifies the table to use for the TB size calculation. The MCS Table, along with the MCS setting, determines the modulation format and coding rate applied to a physical channel transmission. For more details, refer to section 5.1.3 of 38.214.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding > MCS Table

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:MCS:TABLe TABLe51|TABLe52|TABL61|TABLe53|TABL62

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:MCS:TABLe?

SCPI Example

RAD:NR5G:WAV:CCAR0:ULIN:SCH0:MCS:TABL TABL51

Couplings

If Transform Precoding is enabled, the following tables are available.

  • Table 5.1.3.1-2 (256QAM)

  • Table 6.1.4.1-1 (64QAM TP)

  • Table 6.1.4.1-2 (64QAM TP LowSE)

If the input value is not one of the above tables, it is coupled to Table 6.1.4.1-1 (64QAM TP)

If Transform Precoding is disabled, the following tables are available.

  • Table 5.1.3.1-1 (64QAM)

  • Table 5.1.3.1-2 (256QAM)

  • Table 5.1.3.1-3 (64QAMLowSE)

If the input value is not one of the above tables, it is coupled to Table Table 5.1.3.1-1 (64QAM)

Preset

TABL51

State Saved

Yes

MCS

Sets the Modulation and Coding Scheme used for modulation of the data on the physical channel. The MCS setting, along with the MCS Table, determines the modulation format and coding rate applied to a physical channel transmission.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding > MCS

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:MCS <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:MCS? [MAXimum|MINimum]

SCPI Example

 

Couplings

The MCS table is either Table 6.1.4.1-1 (64QAM TP) or Table 5.1.3.1-2 (256QAM) :

Preset

0

State Saved

Yes

Min

-1

Max

28

Resolution

1

xOverhead

Set the xOverhead parameter (N_oh_PRB) to calculate to TB size.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding > xOverhead

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:XOVerhead <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:XOVerhead?

SCPI Example

 

Preset

0

State Saved

Yes

Choices

0 | 6 | 12 | 18

Number of Slots for TBoMS

Transport Block on Multiple Slots (TBoMS), and it used for coverage enhancement in release 17. It applies on PUSCH only.

If "Number of Slot for TBoMS" is 1, it means numberOfSlotsTBoMS is not present in the resource allocation table, or numberOfSlotsTBoMS is present in the resource allocation table and the value of numberOfSlotsTBoMS in the row indicated by the Time domain resource assignment field in DCI is equal to 1. 

If “Number of Slot for TBoMS” is 2, 4, or 8, it means one TB will be mapped to 2, 4, or 8 slots.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding > Number of Slots for TBoMS

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:NSLots?

SCPI Example

 

Preset

1

State Saved

Yes

Choices

1 | 2 | 4 | 8

Start Position for LDPC Rate-Matching

When set to "Auto," the start position of LDPC rate-matching follows the standard. If it is not set to "Auto," it can be an integer array and the length of the array is "Number of Slots for TBoMS."

Example for Start Position for LDPC Rate-Matching:

This setting means 4 slots are sharing one TB and the start position of LDPC rate-matching (k0) are  0 for slot0, 200 for slot 1, 300 for slot2 and 400 for slot3. 

The TBS is limited to one coding block when TBoMS is used. This is defined in 6.2.3 in TS38.212. So when the allocated resource is too large for TBoMS cases, there will be an error message as follows.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding > Start Position for LDPC Rate-Matching

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:SPOSition?

SCPI Example

 

Preset

Auto

State Saved

Yes

Choices

Auto | Number Array separated by “,”

Coding Rate

Displays the coding rate of the channel. It is automatically updated by MCS index change.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding > Coding Rate

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CRATe?

SCPI Example

 

Preset

0.1171875

State Saved

Yes

Modulation

Displays the modulation type of the channel. It is automatically updated by an MCS index change.

Choices:

When Channel Coding is off and MCS is -1: pi/2 BPSK, QPSK, 8PSK, 16QAM, 64QAM, 256QAM, 1024QAM, User Defined

When Transform Precoding is on, MCS is 0 or 1, and MCS Table is 6.1.4.1-1: pi/2 BPSK or QPSK

When Channel Coding is off and MCS is -1, you can select a modulation type.

When Transform Precoding is on, MCS is 0 or 1, and MCS Table is 6.1.4.1-1 you can select a modulation type.

When User Defined is selected, the User Defined Constellation field appears below.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding > Modulation

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:MODulation PIBPsk|QPSK|QAM16|QAM64|QAM256

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:MODulation?

SCPI Example

 

Preset

QPSK

State Saved

Yes

Choices

PI/2 BPSK | QPSK |QAM16 | QAM64 | QAM256

User Defined Constellation

To see this function, Channel Coding must be off and MCS must be set to -1.

User Defined Constellation accepts a text string that you can enter directly into the parameter field or create by using an editor, accessed by clicking the arrow button.

Preset

Opens a menu where you can select a preset constellation.

Choices: OOK, 2ASK, 4ASK, 8ASK, BPSK, QPSK, 8PSK, 16APSK, 16QAM, 32QAM, 64QAM, 128QAM, 256QAM, 512QAM, 1024QAM, 2048QAM, 4096QAM

Insert

Inserts a new symbol row after the selected symbol row. The inserted symbol is 0+0i by default.

Click the area left of the # number to select the symbol row. .

Delete

Delete the selected symbol row.

Click the area left of the # number to select the symbol row. .

Recall

Recall a constellation by opening a .txt file. The format is saved as that defined in Custom Modulation Plugin and described in 2.4.3 of this document.

Save

Save the constellation to a text file. The format of the text file string is defined in Format of the Constellation String

Normalize

Scale the I/Q value to make the average power of all symbols in the constellation to be 1.

Format of the Constellation String

The format of the string is compatible with Custom Modulation. The string is separated by “;” or “\r\n”. Each line or part represents a symbol state defined in the constellation. The values for each symbol should be separated with commas and include Index , I (real) , Q (imaginary) , and Symbol in that order. Magnitude and phase are not included, as they are calculated from the I and Q values. The example below shows the symbols for an 8PSK constellation as they appear in the text file. You can also generate this type of file with other tools, such as Matlab.

0,1.00000,0.00000,0

1,0.70711,0.70711,1

2,0.00000,1.00000,2

3,-0.70711,0.70711,3

4,-1.00000,0.00000,4

5,-0.70711,-0.70711,5

6,0.00000,-1.00000,6

7,0.70711,-0.70711,7

I values and Q values are in double format. Symbols are in hexadecimal format.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding > User Defined Constellation

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CONStln:USER <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CONStln:USER?

SCPI Example

 

State Saved

Yes

Transport Block Size

Displays the transport block size of the channel. It's automatically updated by MCS index change.

The Xoh-PUSCH parameter is assumed to 0.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding > Transport Block Size

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:TB:SIZE?

SCPI Example

 

Couplings

Coupled with Coding Rate, Modulation, DMRS Configuration, Symbol Number, Number of DMRS CDM Group Without Data, RA Type, RB Number, Number of Layers, BWP, MCS and MCS Table.

Preset

9984

State Saved

Yes

BaseGraph

Displays the base graph of the channel. It is automatically updated by an MCS index change.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding > BaseGraph

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:BGRaph?

SCPI Example

 

Couplings

If Transport Block Size <= 292 or (Transport Block Size <=3824 and Coding Rate <=0.67 or Coding Rate <=0.25

The value is set to 2

Otherwise:

    The value is set to 1

Preset

2

State Saved

Yes

LBRM

Set the LBRM for coding.

Limited-Buffer Rate Matching (LBRM) is a technique used to execute Hybrid Automatic Repeat reQuest (HARQ) with reduced requirements for soft buffer sizes while maintaining the peak data rates. LBRM shortens the length of the virtual circular buffer of the code block segments for certain large sizes of Transport Block (TB), and therefore sets a lower bound on the code rate.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding > LBRM

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:LBRM[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:LBRM[:STATe]?

SCPI Example

 

Preset

Off

State Saved

No

Payload Data

Opens the Payload Data where you can select a payload data type. You can also create a custom pattern or load a user file.

Payload Data

Seeds

Inverted

Generated sequence begins with...

PN9

All 1s

No

111111111…

PN15

All 1s

Yes

000000000000000…

PN23

All 1s

Yes

00000000000000000000000…

PN31

All 1s

Yes

0000000000000000000000000000000…

See also Using Custom Payload Data for more information.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding > Payload Data

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DATA:TYPE PN9|PN15|PN23|CUSTom|FILE

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DATA:TYPE?

SCPI Example

 

Choices

PN9 | PN15 | PN23 | PN31 | Custom Pattern | User File

Preset

PN9

State Saved

Yes

Custom Pattern

Opens an editor so you can create and save customized payload data.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding > Payload Data > Custom Pattern

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DATA <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DATA?

SCPI Example

 

Preset ""

State Saved

Yes

User File

Opens a dialog so you can select a previously saved payload data file.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding > Payload Data > User File

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DATA:FILE <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DATA:FILE?

SCPI Example

 

Preset

""

State Saved

Yes

Modulation and Coding (Transport Block 2)

The functions in the Modulation and Coding (Transport Block 2) set are specifically for MIMO configurations. This tab and its settings are only available when the Number of Codewords is 2. Two codewords are supported when UL-SCH > Transmission Settings > DMRS port(s) value is greater than four (for example: 0,1,2,3,4,5).

MCS #2

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding (Transport Block 2) > MCS #2

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH:TB2:MCS <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH:TB2:MCS?

SCPI Example

 

Preset

0

Min 0
Max 28

State Saved

Yes

Coding Rate #2

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding (Transport Block 2) > Coding Rate #2

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH:TB2:CRATe?

SCPI Example

 

Preset

0.1171875

State Saved

Yes

Modulation #2

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding (Transport Block 2) > Modulation #2

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH:TB2:MODulation?

SCPI Example

 
Choices PIBPsk | QPSK | QAM16 | QAM64 | QAM256 | QAM1024 | USER

Preset

QPSK

State Saved

Yes

Transport Block Size #2

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding (Transport Block 2) > Transport Block Size #2

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH:TB2:SIZE?

SCPI Example

 

Preset

29736

State Saved

Yes

BaseGraph #2

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding (Transport Block 2) > BaseGraph #2

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH:TB2:BGRaph?

SCPI Example

 

Preset

2

State Saved

Yes

Payload Data #2

Opens the Payload Data where you can select a payload data type. You can also create a custom pattern or load a user file.

Payload Data

Seeds

Inverted

Generated sequence begins with...

PN9

All 1s

No

111111111…

PN15

All 1s

Yes

000000000000000…

PN23

All 1s

Yes

00000000000000000000000…

PN31

All 1s

Yes

0000000000000000000000000000000…

See also Using Custom Payload Data for more information.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding (Transport Block 2) > Payload Data #2

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH:TB2:DATA:TYPE PN9|PN15|PN23|PN31|CUSTom|FILE

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH:TB2:DATA:TYPE?

SCPI Example

 

Preset

PN9

State Saved

Yes

Custom Pattern

To see/use this function, set Payload Data #2 to Custom Pattern.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding (Transport Block 2) > Payload Data #2 > Custom Pattern

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH:TB2:DATA <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH:TB2:DATA?

SCPI Example

 

State Saved

Yes

User File

To see/use this function, set Payload Data #2 to User File.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > Modulation and Coding (Transport Block 2) > Payload Data #2 > User File

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH:TB2:DATA:FILE <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH:TB2:DATA:FILE?

SCPI Example

 

State Saved

Yes

HARQ Settings

RV index

Sets the redundancy version index of PDSCH for the transmission. Refer to 3GPP 38.212 for more details.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > HARQ Settings > RV Index

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:RV:INDex <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:RV:INDex?

SCPI Example

 

Preset

0

State Saved

Yes

Min

0

Max

3

Resolution

1

CBG Transmission

Enables or Disables a CBG transmission.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > HARQ Settings > CBG Transmission

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CBG[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CBG[:STATe]?

SCPI Example

 

Preset

Off

State Saved

Yes

Max CBGs Per TB

Sets the maxCodeBlockGroupsPerTransportBlock when CBG transmission is enabled.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > HARQ Settings > Max CBGs Per TB

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CBG:MAX <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CBG:MAX?

SCPI Example

 

Preset

8

State Saved

Yes

CBG Transmission Information

Enter a one-zero string to set the CBG transmission information for re-transmission whenCBG transmission enabled, the length of string is MaxCBGsPerTB.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > HARQ Settings > CBG Transmission Information

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CBG:TI <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CBG:TI?

SCPI Example

 

Preset

11111111

State Saved

Yes

CRC Error Flag

Enter an one-zero string to set the whether CRC error is inserted for current TB or CBG. For CBG transmission enabled, the length of string is MaxCBGsPerTB, for CBG transmission disabled, the length of string is 1.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > HARQ Settings > CRC Error Flag

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CRC:ERRor <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CRC:ERRor?

SCPI Example

 

Preset

0

State Saved

Yes

DMRS Settings

DMRS-Uplink-r16

Enables or disables whether higher-layer parameter DMRS-Uplink-r16 is provided.

Transform Precoding must be disabled for this parameter to appear.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > DMRS Settings > DMRS-Uplink-r16

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:TP16ul[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:TP16ul[:STATe]?

SCPI Example

 

Preset

Off

State Saved

Yes

DMRS-UplinkTransformPrecoding-r16

Enables or disables whether higher-layer parameter DMRS-UplinkTransformPrecoding-r16 is provided.

Transform Precoding must be enabled for this parameter to appear.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > DMRS Settings > DMRS-UplinkTransformPrecoding-r16

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:TP16ul[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:TP16ul[:STATe]?

SCPI Example

 

Preset

Off

State Saved

Yes

n_SCID

Sets the n_SCID for sequence generation.

This function is only available when UL-SCH > General Settings > Transform Precoding is set to Off.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > DMRS Settings > N_SCID

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:SCIDn <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:SCIDn?

SCPI Example

 

Preset

0

State Saved

Yes

Min

0

Max

1

N_ID_0

Sets the N_ID_nSCID (N_ID_0 or N_ID_1) for sequence generation, -1 means cell ID.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > DMRS Settings > N_ID_0

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:NID0 <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:NID0?

SCPI Example

 

Preset

-1

State Saved

Yes

Min

-1

Max

65535

N_ID_1

Sets the N_ID_nSCID (N_ID_0 or N_ID_1) for sequence generation, -1 means cell ID.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > DMRS Settings > N_ID_1

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:NID1 <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:NID1?

SCPI Example

 

Preset

-1

State Saved

Yes

Min

-1

Max

65535

DMRS Power Boosting

Specifies the DMRS power boosting relative to the data part. When the number of DMRS CDM groups without data is changed, the DMRS power boosting is automatically changed based on the Table 4.1-1 of 38.214.

When the number of DMRS CDM groups without data is changed, the DMRS power boosting is automatically changed based on the Table 4.1-1 of 38.214.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > DMRS Settings > DMRS Power Boosting

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:POWer <rel_ampl>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:POWer? [MAXimum|MINimum]

SCPI Example

 

Couplings

If the number of DMRS CDM Group Without Data = 1

Value is 0 dB

If the number of DMRS CDM Group Without Data = 2

Value is 3 dB

If the number of DMRS CDM Group Without Data = 1

Value is 4.77 dB

Preset

0.00 dB

State Saved

 

Min

-40 dB

Max

40 dB

Resolution

0.01 dB

DMRS Configuration

Sets the DMRS Configuration for the channel. When Transform Precoding (UL-SCH) > General Settings > Transform Precoding) is enabled, DMRS Configuration is set to Type 1. When Transform Precoding is disabled, the value can be set to Type 1 or Type 2.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > DMRS Settings > DMRS Configuration

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:CONFigure TYPE1|TYPE2

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:CONFigure?

SCPI Example

 

Preset

TYPE1

State Saved

Yes

DMRS Duration

Specifies the DMRS duration for the channel. The DMRS duration can be one symbol or two symbols.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > DMRS Settings > DMRS Duration

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:DURation SINGle|DOUBle

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:DURation?

SCPI Example

 

Preset

Single

State Saved

Yes

Enhanced DMRS Type

Requires license version 2024.0801 or later.

When Enhanced DMRS Type is set to ON, the DMRS ports can be configured as follows.

DMRS multiplexing

DMRS duration

Supported DMRS ports

  Configuration Type 1 Configuration Type 2

Basic

Single-symbol 0 - 3 0 - 5
Double-symbol 0 - 7 0 - 11

Enhanced (Rel-18)

Single-symbol 0 - 3, 8 - 11 0 - 5, 12 - 17
Double-symbol 0 - 15 0 - 23

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > DMRS Settings > Enhanced DMRS Type

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH:DMRS:EDTYpe[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH:DMRS:EDTYpe[:STATe]?

SCPI Example

RAD:NR5G:WAV:CCAR0:ULIN:SCH:DMRS:EDTY 1

Preset

OFF

State Saved

Yes

DMRS-add-pos

Sets a value indicating the additional DMRS positions for this channel. The range is based on the Symbol Number, DMRS Duration, Mapping Type, and DMRS-typeA-pos. Refer to 6.4.1.1.3 of 38.211 for more details.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > DMRS Settings > DMRS-add-pos

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:APOS <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:APOS?

SCPI Example

 

Couplings

When the DMRS Duration is a Single Symbol, the maximum value is 3.

When the DMRS Duration is a Double Symbol, the maximum value is 1.

Preset

0

Min

0

Max

3

Resolution

1

PUSCH Mapping

Sets the PUSCH mapping type. Valid PUSCH allocations are based on table 6.1.2.1-1 of the 5G NR standard. S = start symbol index and L = number of consecutive symbols.

PUSCH mapping type

Normal cyclic prefix

Extended cyclic prefix

S

L

S+L

S

L

S+L

Type A

0

{4,...,14}

{4,...,14}

0

{4,...,12}

{4,...,12}

Type B

{0,...,13}

{1,...,14}

{1,...,14}

{0,...,12}

{1,...,12}

{1,...,12}

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > DMRS Settings > PUSCH Mapping

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:PUSCh:MAPPing TYPEA|TYPEB

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:PUSCh:MAPPing?

SCPI Example

 

Preset

TYPEA

State Saved

Yes

DMRS-typeA-pos

Sets the PUSCH DMRS position for mapping type A to either Pos2 or Pos3.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > DMRS Settings > DMRS-typeA-pos

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:TAPos <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:TAPos?

SCPI Example

 

Preset

2

Min

2

Max

3

State Saved

Yes

n_ID_RS

Set the n_ID_RS for the DMRS generation.

This function is only available when UL-SCH > General Settings > Transform Precoding is set to On.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > DMRS Settings > n_ID_RS

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:RSIDn <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:RSIDn?

SCPI Example

 

Preset

-1

State Saved

Yes

Min

-1

Max

65535

Resolution

1

Group Hopping

Enables or disables group hopping for sequence generation.

This function is only available when UL-SCH > General Settings > Transform Precoding is set to On.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > DMRS Settings > Group Hopping

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:GHOPping[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:GHOPping[:STATe]?

SCPI Example

 

Preset

Off

State Saved

Yes

Sequence Hopping

Enables or disables sequence hopping for sequence generation.

This function is only available when UL-SCH > General Settings > Transform Precoding is set to On.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > DMRS Settings > Sequence Hopping

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:SHOPping[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:DMRS:SHOPping[:STATe]?

SCPI Example

 

Preset

Off

State Saved

Yes

PTRS Settings

PTRS Enabled

Enables or disables the PTRS state.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > PTRS Settings > PTRS Enabled

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:PTRS[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:PTRS[:STATe]?

SCPI Example

 

Preset

Off

State Saved

Yes

PTRS PowerBoosting

Sets the relative power boosting (in dB) of the PTRS associated with the PUSCH physical channel. This is a power scaling based on the constellation defined in 5.1.3/4/5/6 of 38.211.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > PTRS Settings > PTRS Power Boosting

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:PTRS:POWer <rel_ampl>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:PTRS:POWer?

SCPI Example

 

Preset

0.00 dB

State Saved

Yes

Min

-40 dB

Max

40 dB

Resolution

0.01 dB

PTRS port(s)

Sets the PTRS ports used. The maximum number is 2.

This function is only available when UL-SCH > General Settings > Transform Precoding is set to Off.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > PTRS Settings > PTRS Ports

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:PTRS:PORTs <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:PTRS:PORTs?

SCPI Example

 

Preset

"0"

State Saved

Yes

Frequency Density (K_PTRS)

Sets the PTRS period in subcarrier in the frequency domain.

This function is only available when UL-SCH > General Settings > Transform Precoding is set to Off.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > PTRS Settings > Frequency Density

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:PTRS:FREQuency:DENSity <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:PTRS:FREQuency:DENSity?

SCPI Example

 

Preset

2

State Saved

Yes

Min

2

Max

4

Time Density (L_PTRS)

Sets the start PTRS symbol in time domain.

This function is only available when UL-SCH > General Settings > Transform Precoding is set to Off.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > PTRS Settings > Time Density

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:PTRS:TIME:DENSity <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:PTRS:TIME:DENSity?

SCPI Example

 

Notes

Only 1,2 and 4 are valid values.

Preset

1

State Saved

Yes

PTRS RE Offset

Sets the PTRS resource element offset.

This function is only available when UL-SCH > General Settings > Transform Precoding is set to Off.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > PTRS Settings > PTRS RE Offset

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:PTRS:RE:OFFSet OFFS00|OFFS01|OFFS10|OFFS11

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:PTRS:RE:OFFSet?

SCPI Example

 

Notes

Only 00, 01, 10 and 11 are valid values.

Preset

OFFS00 or 00

State Saved

Yes

Number of samples per PT-RS group

Sets the Number of samples per PT-RS group (N_samp_group) for PTRS signal generation.

This function is only available when UL-SCH > General Settings > Transform Precoding is set to On.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > PTRS Settings > Number of Samples Per PTRS Group

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:PTRS:GROup:SAMPle:COUNt <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:PTRS:GROup:SAMPle:COUNt?

SCPI Example

 

Notes

Only 2 and 4 are valid values.

Preset

2

State Saved

Yes

Number of PT-RS groups

Sets the Number of PT-RS groups (N_samp_group) for PTRS signal generation.

This function is only available when UL-SCH > General Settings > Transform Precoding is set to On.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > PTRS Settings > Number of PTRS Groups

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:PTRS:GROup:COUNt <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:PTRS:GROup:COUNt?

SCPI Example

 

Notes

Only 2, 4 and 8 are valid value.

Preset

2

State Saved

Yes

N_ID

Sets the N_ID for the PTRS generation when transform precoding is enabled.

This function is only available when UL-SCH > General Settings > Transform Precoding is set to On.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > PTRS Settings > N_ID

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:PTRS:NID <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:PTRS:NID?

SCPI Example

 

Preset

0

State Saved

Yes

Min

0

Max

65535

Resolution

1

UCI on PUSCH

The Uplink Control Information (UCI) is carried by PUSCH (or PUCCH). The information carried on the UCI includes:

UL-SCH Enabled

Enables or disables UL-SCH when UCI is multiplexed with UL-SCH.

It is set to On if no UCI is transmitted on UL-SCH.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > UCI on PUSCH > UL-SCH Enabled

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI[:STATe]?

SCPI Example

 

Preset

On

State Saved

Yes

uci-on-pusch-scaling

Sets the UCI on PUSCH scaling when UCI is multiplexed with UL-SCH. This is used to limit the number of resource elements assigned to UCI on PUSCH. See TS 38.212, Section 6.3.2.4 for more information.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > UCI on PUSCH > uci-on-pusch-scaling

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:SCALing <real>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:SCH<channel>:UCI:SCALing?

SCPI Example

 

Choices

0.5 | 0.65 | 0.8 | 1

Preset

0.5

HARQ-ACK

Enabled

Enables or disables HARQ-ACK multiplexing for UL-SCH.Hybrid Automatic Repeat Request Acknowledgment (HARQ-ACK) is the information a receiver feeds back to the transmitter in order to acknowledge the correct reception of a packet or ask for a new re-transmission.

This function is only available when UL-SCH > Modulation and Coding > Channel Coding is On.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > HARQ-ACK > Enabled

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:HACK[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:HACK[:STATe]?

SCPI Example

 

Preset

Off

State Saved

Yes

Payload Data

This function is only available when HARQ-ACK is enabled.

Opens the Payload Data where you can select a payload data type. You can also create a custom pattern or load a user file.

Payload Data

Seeds

Inverted

Generated sequence begins with...

PN9

All 1s

No

111111111…

PN15

All 1s

Yes

000000000000000…

PN23

All 1s

Yes

00000000000000000000000…

PN31

All 1s

Yes

0000000000000000000000000000000…

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > HARQ-ACK > Payload Data

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:HACK:DATA:TYPE PN9|PN15|PN23|CUSTom|FILE

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:HACK:DATA:TYPE?

SCPI Example

 

Choices

PN9 | PN15 | PN23 | PN31 | Custom Pattern | User File

Preset

PN9

State Saved

Yes

Custom Pattern

Opens an editor so you can create and save customized payload data.

See also Using Custom Payload Data for more information.

This function is only available when HARQ-ACK is enabled.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > HARQ-ACK > Payload Data set to Custom Pattern

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:HACK:DATA <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>|1|2|3|4|5|6|7:UCI:HACK:DATA?

SCPI Example

 

Preset

""

State Saved

Yes

User File

Opens a dialog so you can select a previously saved payload data file.

See also Using Custom Payload Data for more information.

This function is only available when HARQ-ACK is enabled.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > HARQ-ACK > Payload Data set to User File

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:HACK:DATA:FILE <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:HACK:DATA:FILE?

SCPI Example

 

Preset

""

State Saved

Yes

Payload Size

Sets the HARQ-ACK payload size before channel coding.

This function is only available when HARQ-ACK is enabled.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > HARQ-ACK > Payload Size

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:HACK:DATA:LENGth <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:HACK:DATA:LENGth?

SCPI Example

 

Preset

10

Min

1

Max

200

Resolution

1

BetaOffsetIndex

Sets the beta offset index of UCI when multiplexing with UL-SCH.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > HARQ-ACK > BetaOffsetIndex

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:HACK:BOINdex <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:HACK:BOINdex? [MAXimum|MINimum]

SCPI Example

 

Preset

0

Min

0

Max

15

Resolution

1

State Saved

Yes

CSI1 or CSI2

Enabled

Enables or disables CSI multiplexing with UL-SCH. Channel State Information (CSI) describes characteristics of the radio channel. It usually indicates the complex transfer function matrix between one or more transmitting antennas and one or more receiving antennas.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > CSI1 or CSI2 > Enabled

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:CSI1|2[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:CSI1|2[:STATe]?

SCPI Example

 

Notes

Cardinality of CSI starts from 1 for consistency with the standard and GUI

Preset

Off

State Saved

Yes

Payload Data

CSI must be enabled to use this function.

Opens the Payload Data where you can select a payload data type. You can also create a custom pattern or load a user file.

Payload Data

Seeds

Inverted

Generated sequence begins with...

PN9

All 1s

No

111111111…

PN15

All 1s

Yes

000000000000000…

PN23

All 1s

Yes

00000000000000000000000…

PN31

All 1s

Yes

0000000000000000000000000000000…

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > CSI1 or CSI2 > Payload Data

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:CSI1|2:DATA:TYPE PN9|PN15|PN23|CUSTom|FILE

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:CSI1|2:DATA:TYPE?

SCPI Example

 

Notes

Cardinality of CSI starts from 1 for consistency with the standard and GUI

Preset

PN9

State Saved

Yes

Custom Pattern

Opens an editor so you can create and save customized payload data.

See also Using Custom Payload Data for more information.

CSI must be enabled to use this function.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > CSI1 or CSI2 > Payload Data set to Custom Pattern

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:CSI1|2:DATA <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>|1|2|3|4|5|6|7:UCI:CSI1|2:DATA?

SCPI Example

 

Notes

Cardinality of CSI starts from 1 for consistency with the standard and GUI

Preset

""

State Saved

Yes

User File

Opens a dialog so you can select a previously saved payload data file.

See also Using Custom Payload Data for more information.

CSI must be enabled to use this function.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > CSI1 or CSI2 > Payload Data set to User File

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:CSI1|2:DATA:FILE <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:CSI1|2:DATA:FILE?

SCPI Example

 

Notes

Cardinality of CSI starts from 1 for consistency with the standard and GUI

Preset

""

State Saved

Yes

Payload Size

Sets the CSI payload size before channel coding.

CSI must be enabled to use this function.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > CSI1 or CSI2 > Payload Size

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:CSI1|2:DATA:LENGth <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:CSI1|2:DATA:LENGth?

SCPI Example

 

Notes

Cardinality of CSI starts from 1 for consistency with the standard and GUI

Preset

10

Min

1

Max

200

Resolution

1

BetaOffsetIndex

Sets the beta offset index of UCI when multiplexing with UL-SCH.

CSI must be enabled to use this function.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > CSI1 or CSI2 > BetaOffsetIndex

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:CSI1|2:BOINdex <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:UCI:CSI1|2:BOINdex? [MAXimum|MINimum]

SCPI Example

 

Notes

Cardinality of CSI starts from 1 for consistency with the standard and GUI

Preset

0

Min

0

Max

18

Resolution

1

State Saved

Yes

CG-UCI

Enabled

Enables or Disables CG-UCI multiplexing with UL-SCH.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > CG-UCI > Enabled

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CGUCi[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CGUCi[:STATe]?

SCPI Example

 

Preset

Off

State Saved

Yes

Payload Data

CG-UCI must be enabled to use this function.

Opens the Payload Data where you can select a payload data type. You can also create a custom pattern or load a user file.

Payload Data

Seeds

Inverted

Generated sequence begins with...

PN9

All 1s

No

111111111…

PN15

All 1s

Yes

000000000000000…

PN23

All 1s

Yes

00000000000000000000000…

PN31

All 1s

Yes

0000000000000000000000000000000…

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > CG-UCI > Payload Data

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CGUCi:DATA:TYPE PN9|PN15|PN23|PN31|CUSTom|FILE

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CGUCi:DATA:TYPE?

SCPI Example

 

Preset

PN9

State Saved

Yes

Custom Pattern

Opens an editor so you can create and save customized payload data.

CG-UCI must be enabled to use this function.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > CG-UCI > Payload Data set to Custom Pattern

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CGUCi:DATA <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CGUCi:DATA?

SCPI Example

 

Preset

 

State Saved

Yes

User File

Opens a dialog so you can select a previously saved payload data file.

CG-UCI must be enabled to use this function.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > CG-UCI > Payload Data set to User File

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CGUCi:DATA:FILE <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CGUCi:DATA:FILE?

SCPI Example

 

State Saved

Yes

Payload Size

Sets the CG-UCI payload size before channel coding.

CG-UCI must be enabled to use this function.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > CG-UCI > Payload Size

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CGUCi:DATA:LENGth <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CGUCi:DATA:LENGth?

SCPI Example

 

Preset

10

State Saved

Yes

BetaOffsetIndex

Sets the beta offset index of UCI when multiplexing with UL-SCH.

CG-UCI must be enabled to use this function.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > UL-SCH > CG-UCI > BetaOffsetIndex

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CGUCi:BOINdex <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:SCH<channel>:CGUCi:BOINdex?

SCPI Example

 

Preset

0

State Saved

Yes

Min 0
Max 18

Carrier Uplink